Technical FAQs

Ask a Question

What are the standard lugs supplied with the 600 amp or 800 amp PGL, PJL, PLL unit mount breaker and what wire sizes do these lugs accommodate?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
The standard lugs are AL800M23K. The qty (3) lugs which are supplied with this kit each accommodate (3) #3/0 through 500 kcmil AL/CU.


CTA-ID : 2044797
Was this helpful?
What can we do to improve the information ?