Technical FAQs

Ask a Question

Can the Class 8502 Type SBG__ contactor be converted to a 8536 starter by adding 9065SDO__ or 9065SS__ overload relay and 9066SC1 external reset mechanism?

The open style contactor can be modified by adding the appropriate overload relay however there are no provisions provided on the enclosure cover for mounting the 9066SC1 external reset mechanism. The solid state overload can only be used on three phase power systems.


CTA-ID : 2044865
Was this helpful?
What can we do to improve the information ?