Technical FAQs

Ask a Question

What is the suffix A06G on an IEC combination starter?

It is the addition of a Start Stop push button.


CTA-ID : 2044761
Was this helpful?
What can we do to improve the information ?