Technical FAQs

Ask a Question

What is the replacement for the Q22200P breaker?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
The replacement breaker is obsolete, no longer available with no replacement.
Q22200P was a special 200A 2P Q2 breaker built for HITCH-N-POST METER PEDESTALS units. The complete unit HNP2200CB, which included the breaker is also obsolete, no longer available with no Replacement.


CTA-ID : 2044622
Was this helpful?
What can we do to improve the information ?