Technical FAQs

Ask a Question

What is the catalog number for the handle padlock attachment for a Q4 breaker?

Issue:
What is the catalog number for the handle padlock attachment for a Q4 breaker?

Product Line:
LA/LH and Q4 breakers

Environment:
This applies to legacy LA/LH and Q4 breakers

Cause:
Need a padlock attachment for the LA/LH/Q4 breaker.

Resolution:
Part number is HPALM for the standard handle and HPAXLM for use with the handle extension (AHEXLI). Both HPALM and HPAXLM can lock the handle in the ON or OFF position and is fixed on the front of the breaker when added .


CTA-ID : 2044011
Was this helpful?
What can we do to improve the information ?