Technical FAQs

Ask a Question

What are the voltage tolerances for a shunt trip coil accessory, suffix 1021?

Product Line:
Legacy type circuit breakers

Electrical Distribution Equipment

The voltage tolerance for the 1021 shunt trip is 55% to 110% of rated voltage.

CTA-ID : 2043795
Was this helpful?
What can we do to improve the information ?