Technical FAQs

Ask a Question

What is the plastic cover that swings out on an MCC model 6 that holds the Start/Stop pushbuttons, 22mm or 30mm

Issue:
What is the plastic cover that swings out on an MCC model 6 that holds the Start/Stop pushbuttons,  22mm or 30mm

Product Line:
Model 6 motor control center.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Advised customer that for the 22mm 5 device Control station panel, replacement part number is 80420-007-05. For the 30mm 3 device Station control panel, replacement part number is 80420-007-06


CTA-ID : 2030869
Was this helpful?
What can we do to improve the information ?