Technical FAQs

Ask a Question

What is the replacement power contact kit part number for Class 8502 or Class 8536 Type SC** contactor or starter?

Product Line:
 
NEMA Type S Replacement Part Kits
 
Resolution:
 
3-Pole Kit 9998 SL3, 4-Pole Kit 9998 SL13.

This also applies to all 8536 SC, 8538 SC, 8539 SC, 8630 SC, 8640 SC, 8702 SC, 8736 SC, 8738 SC, 8739 SC, 8810 SC, 8810CC, 8810 UC, 8810 DC, 8903 SM, 8940 Size 1 except ``NP``, 8941 NC, 8941 CC, 8941 UC, and 8941 DC devices.


CTA-ID : 2043993
Was this helpful?
What can we do to improve the information ?