Technical FAQs

Ask a Question

8536SHO2 Size 6 Starter: What does the control module (31123-514-50) do?

Issue:      
What is the control module used for

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause: Identifying application


Resolution:
It converts 120VAC control voltage to DC voltages to feed the DC coil of the contactor. It will give the coil 100-140V DC for starting and then drop the voltage to 8-13V DC for holding.


CTA-ID : 2043931
Was this helpful?
What can we do to improve the information ?