Technical FAQs

Ask a Question

What is the part number for the mounting bracket that holds the start stop pushbutton in place for the 8502, 8536, size 00, 0, 1, 2, or 3 in standard Nema 1 enclosures?

Product Line:

NEMA style Contactors and Starters

Resolution:
 
The plastic mounting bracket is part number 31033-016-01. This is also the bracket that is removed when this kit is used on 8538 and 8539 combos.


CTA-ID : 2044491
Was this helpful?
What can we do to improve the information ?