Technical FAQs

Ask a Question

Is it possible to order an 8910DPA type contactor without the Sta-Con or Fast-On connectors?

Yes. Use the U1 form at the end of the catalog number. For example: 8910DPA43V02U1, or 8910DPA53V02U1. The form U1 removes the Sta-Con or Fast-On connectors. This also causes the device to become UL listed rather than component recognized.


CTA-ID : 2046265
Was this helpful?
What can we do to improve the information ?