Technical FAQs

Ask a Question

Can a two pole breaker be used in the catalog number QMBJW, QMB panelboard circuit breaker adapter?

No. This QMB Switchboard or Panelboard circuit breaker adapter is UL Listed to utilize only three pole breakers.


CTA-ID : 2046292
Was this helpful?
What can we do to improve the information ?