Technical FAQs

Ask a Question

What is the replacement handle extension for a Merlin Gerin Compact NSJ400N, NSJ600N, NS400, or NS600?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
Part # 32553 is for one extension handle which is obsolete and no longer available.  Part number S432553 is new number and includes (5) extensions.

Note: The original handle is not replaceable and if it is broken.


CTA-ID : 2046615
Was this helpful?
What can we do to improve the information ?