Technical FAQs

Ask a Question

What is the SCCR (Short Circuit Current Rating) for a HU368, HU368AWK or HU368R non-fusible safety switch?

Issue:
Application

Product Line:
HD Safety Switch

Cause:
Application regarding SCCR

Resolution:
These switches are suitable for use on a circuit capable of delivering not more than 200,000 rms symmetrical amperes, 600Vac maximum, when protected upstream by Class L or Class T fuses rated 1200 ampere maximum. 


CTA-ID : 2045402
Was this helpful?
What can we do to improve the information ?