Technical FAQs

Ask a Question

What is the difference between the GV7AC021 and the GV7AC022? Do I need to order them with the GV7 starters?

Yes, if you need lugs. The GV7AC021 is for the GV7R*40 through GV7R*150 starter. The GV7AC022 is for the GV7R*220 starter. The GV7R*20 and GV7R*25 come with lugs included.


CTA-ID : 2045673
Was this helpful?
What can we do to improve the information ?