Technical FAQs

Ask a Question

Is it possible to obtain a Heavy Duty Safety Switch with a second coat of standard ANSI 49 gray paint?

Issue:
Special options

Product Line:
Heavy Duty Safety Switch

Environment:
Special paint option

Cause:
Request for special paint

Resolution:
Yes, by adding suffix SP8 to the standard catalog number, an overspray coat of ANSI 49 gray paint can be provided. A minimum quantity of 10 is required. Not available on Type 4/4X/5 stainless steel, Type 4X fiberglass or Type 7/9 cast aluminum safety switches.


CTA-ID : 2045681
Was this helpful?
What can we do to improve the information ?