Technical FAQs

Ask a Question

Will the new LA1KN22 auxiliary contacts fit on the old contactor/relay that used the LA1EN22 auxiliary contacts?

No. The LA1KN22 in not compatible with the old contactor/relays. The customer will have to replace the contactor/relay also.


CTA-ID : 2045622
Was this helpful?
What can we do to improve the information ?