Technical FAQs

Ask a Question

Can I use an 8502 Type SE Size 3 contactor to replace the contactor in an 8536 Type SE Size 3 starter?<br />

No. The load side on the 8502 contactor will have lughs and will not match up with line side bussing of the overload relay. The baseplate will also be incorrect.

CTA-ID : 2045806
Was this helpful?
What can we do to improve the information ?