Technical FAQs

Ask a Question

What is the replacement for a QMQB1022?<br />

Contact field service for a paid retrofit, to modify a 600 volt switch to a 240 volt, 2 pole device.
The QMQB1022 has a blank empty section and the present 600V switch will have two switches
If a twin device is OK then the load base needs to be re-located to the 240 volt position and
inter-phase barrier changed. Lugs and fuse clips are to be removed from the center pole.
Mounting hardware may be required and service can evaluate this at site.
Customer needs to contact Schneider Service, this work is not be done by the customer/contractor.



CTA-ID : 2047027
Was this helpful?
What can we do to improve the information ?