Technical FAQs

Ask a Question

What is 31041-402-01?

This was a dual voltage coil 115V or 230V, 60Hz for 8502/8536 Size 00, 0, and 1 contactors/starters. This coil is obsolete. Order a 120V coil as 31041-400-42, or a 240V coil as 31041-400-51.

CTA-ID : 2047669
Was this helpful?
What can we do to improve the information ?