Technical FAQs

Ask a Question

What is 31041-402-04?

This was a dual voltage coil 240V or 480V, 60Hz for 8502/8536 Size 00, 0, and 1 contactors/starters. This coil is obsolete. Order a 240V coil as 31041-400-51 or a 480V coil as 31041-400-60.

CTA-ID : 2047671
Was this helpful?
What can we do to improve the information ?