Technical FAQs

Ask a Question

Can a 60-Blank QMB switch be modified to a 60-60?

No, the blank unit cannot be converted to a switch. If there are any plans to add circuits later, a 60-60 twin switch should be used.

 
Was this helpful?
What can we do to improve the information ?