Technical FAQs

Ask a Question

Is it possible to disable or remove GFCI protection from a PJ breaker while in service?<br /><br />

No. There is no way to defeat the ground fault on the P frame breaker when in use, other than to turn up the ground fault all the way to decrease its low end sensitivity. The trip unit could be changed out to one that does not have ground fault capability.


CTA-ID : 2046685
Was this helpful?
What can we do to improve the information ?