Technical FAQs

Ask a Question

What is the replacement for a QMQB3322?

Contact field service for a paid retrofit to modify a 600 volt switch to a 240 volt, 2 pole device.
Fuse clips need to be changed to 240 volt and the fuse load base needs to be repositioned.
Removal of the center lugs and fuse clips are required. Mounting hardware may be required and service can evaluate this at site.
Please contact Schneider Electric Service. This work is not to be done by the customer/contractor.



CTA-ID : 2047021
Was this helpful?
What can we do to improve the information ?