Technical FAQs

Ask a Question

What is the replacement for a QMQB8022?

Contact field service for a paid retrofit, to modify a 600 volt switch to a 240 volt, 2 pole device.
Reposition load base to the 240V location and remove lugs from the centre pole.
Mounting hardware may be required and service can evaluate this at site.
Customer needs to contact Schneider Service, this work is not to be done by the customer/contractor.



CTA-ID : 2047031
Was this helpful?
What can we do to improve the information ?