Technical FAQs

Ask a Question

What is the replacement for a QMQB1122?

Contact field service for a paid retrofit, to modify a 600 volt switch to a 240 volt, 2 pole device.
Load base needs to be re-located to the 240V position and inter-phase barrier changed.
Lugs and fuse clips are to be removed form the centre pole.
Mounting hardware may be required and service can evaluate this at site.
Customer needs to contact Schneider Service, this work is not to be done by the customer/contractor.

CTA-ID : 2047026
Was this helpful?
What can we do to improve the information ?