Technical FAQs

Ask a Question

Can the Tesys T Motor Management System be used on a DC motor application?

No. DC current does not create a fluctuating magnetic field to generate current on the secondary of the internal CT for the overload to monitor.


CTA-ID : 2046899
Was this helpful?
What can we do to improve the information ?