Technical FAQs

Ask a Question

What is the replacement for a QMQB1032?

Contact field service for a paid retrofit, to modify a 600 volt switch to a 240 volt device.
The QMQB1032 has a blank empty section and the present 600V switch will have two switches
If a twin device is OK then the load base needs to be re-located to the 240 volt position and
inter-phase barrier changed. Mounting hardware may be required and service can evaluate this at
site.
Customer needs to contact Schneider Service, this work is not to be done by the customer/contractor.



CTA-ID : 2047040
Was this helpful?
What can we do to improve the information ?