Technical FAQs

Ask a Question

How do you select EDB type EPD breakers?

Issue:
How do you select EDB type EPD breakers?

Product Line:
PowerPact EDB-EPD, EGB-EPD, EJB-EPD

Environment:
This is for 1P only.

Cause:
Need to choose a 30mA equipment ground fault breaker for the NF panelboard.

Resolution:
Only 1P EDB, EGB, EJB breakers are available with 30 mA ground fault protection. They have a EPD suffix and this feature adds 1P space to the width of the breaker.
 
15 A EDB14015EPD EGB14015EPD EJB14015EPD
20 A EDB14020EPD EGB14020EPD EJB14020EPD
30 A EDB14030EPD EGB14030EPD EJB14030EPD
40 A EDB14040EPD EGB14040EPD EJB14040EPD
50 A EDB14050EPD EGB14050EPD EJB14050EPD
Was this helpful?
What can we do to improve the information ?