Technical FAQs

Ask a Question

Can a 100% rated Powerpact H frame Main breaker be factory installed into a NQ panelboard

Issue:
Can a 100% rated Powerpact H frame main breaker be factory installed into an NQ panelboard?

Product Line:
NQ panelboards and accessories sold and supported in the USA.

Environment:
Application, installation

Cause:
Is a 100% H frame main breaker available for the NQ panelboard line?

Resolution:
No, NQ interiors and boxes are not able to accept these breakers with 100% rating feature


CTA-ID : 2048669
Was this helpful?
What can we do to improve the information ?