Technical FAQs

Ask a Question

What mechanical and electrical interlock kits are available to field assemble a reversing contactor from the LC1D09 through LC1D38 (9 to 38 amp ) Tesys contactors?

Product Line:
 
Tesys D line Contactors and Accessories
 
Resolution:
 
Use the LAD9R1V kit for mechanical and electrical interlocking or use the LAD9R1 kit for mechanical interlocking without electrical interlocking. Both include power connections


CTA-ID : 2048018
Was this helpful?
What can we do to improve the information ?