Technical FAQs

Ask a Question

Is there a Nema 4 enclosure for the GV2 starters?

Product Line:

Tesys GV Manual Starter and Protectors
 
Resolution:
No. The enclosures are not UL listed and will have IP ratings only.


CTA-ID : 2048752
Was this helpful?
What can we do to improve the information ?