Technical FAQs

Ask a Question

Are field installable auxiliary contacts available for 8903PB lighting contactors?

Issue:     
Are field installable auxiliary contacts available for 8903PB lighting contactors?

Product Line:
8903 type PB lighting contactor

Environment:
Products sold and used in the United States

Cause:
Auxiliary contacts needed for the 8903 type PB lighting contactor

Resolution:
Auxiliary contacts are available as factory installed or field installed;

For (1) normally open and (1) normally closed SPDT contact order from factory using Form X11 or field install by ordering 8903PBX1.

For (2) normally open and (2) normally closed SPDT contact order from factory using Form X22 or field install by ordering 8903PBX2.



CTA-ID : 2048432
Was this helpful?
What can we do to improve the information ?