Technical FAQs

Ask a Question

Can the M Powerpact breaker be reverse fed?<br /><br />

Yes they can. This breaker comes without the restrictive LINE and LOAD side markings. Reference the Class 612 catalog, 0612CT0101.


CTA-ID : 2048016
Was this helpful?
What can we do to improve the information ?