Technical FAQs

Ask a Question

Are vertical hangers on I Line II Busway available for NEMA 3R applications?

Issue:
Are vertical hangers on I Line II Busway available for NEMA 3R applications?

Product Line:
Busway.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Vertical hangars can be used for outdoor applications. Although the busway hangers for I-Line II were specifically designed for NEMA 1 applications, they can be used as a mounting bracket to mount the busway to an outdoor support structure.


CTA-ID : 2048336
Was this helpful?
What can we do to improve the information ?