Technical FAQs

Ask a Question

Are replacement parts and auxiliary accessories still available for the Class 8502/8536 and Class 8702/8736 pre-type S contactors?

Some 31012-400-** (Type A Series B&C size 00 only) coils are still available as they are also used with some active timing relay devices.
** represents ending digits depending upon voltage required.
All other component parts, parts kits, coils, accessories, etc. are obsolete and no longer available.

If a complete replacement device is required or desired, please use the Competitive Cross Reference tool.

CTA-ID : 2049606
Was this helpful?
What can we do to improve the information ?