Technical FAQs

Ask a Question

Do all three phases make and break at the same time on a U-Line Motor Starter? Some competitive products switch only two poles.

Yes. All three phases open or close simultaneously. None of the three poles stay closed. The internal operation of a U-Line Motor Starter is similar to an ordinary three pole contactor.

CTA-ID : 2049133
Was this helpful?
What can we do to improve the information ?