Technical FAQs

Ask a Question

How is a UFP222RD operated ON and OFF?

This device is operated by removing a pullout head from the base assembly. The pullout head is labeled ON and OFF. To prevent loss, once removed the pullout head may be rotated 180 degrees and reinserted into the base assembly with the OFF marking legible (right side up). To reenergize, the pullout head is reinserted into the base assembly with the ON marking legible (right side up).


CTA-ID : 2049195
Was this helpful?
What can we do to improve the information ?