Technical FAQs

Ask a Question

How is the old obsolete AC Disconnect, catalog number UFP222R operated ON and OFF?

Issue:
Design product feature

Product Line:
Air Conditioning Disconnects

Environment:
Operation of the device

Cause:
Disconnecting for maintenance

Resolution:
This device is operated by removing a pullout head from the base assembly. The pullout head is labeled ON and OFF. Then to prevent loss, once removed, the pullout head may be rotated 180 degrees and reinserted into the base assembly with the OFF marking legible (right side up). To re energize, the pullout head is reinserted into the base assembly with the ON marking legible (right side up).
Was this helpful?
What can we do to improve the information ?