Technical FAQs

Ask a Question

What does the suffix S135 mean on a CAD32 IEC relay?<br />

S135 indicates the removal of the integral surge suppressor on a DC unit. This is a set up special, it is not a Form. It is not valid for units not on the system.



CTA-ID : 2049183
Was this helpful?
What can we do to improve the information ?