Technical FAQs

Ask a Question

What is the part number for the MLP II display ?

Issue:
What is the part number for the MLPII Display?

Product Line:
Solid state overloads and accessories.

Enviroment:
Replacement/repair

Cause:
Maintenance

Resolutioon:
9999MLPD also needs a cable to connect to OL 9999CCKIT

REVISION (11/15)   
The 9999CCKIT is now obsolete, along with the cable for the kit is also obsolete. They will need a 5 wire communication cable.They need to get 2 feet of Belden cable # 8445. They will also need two 5 point terminal connectors. Phoenix terminal block part number 651-1757048, and a 9v battery connector.




CTA-ID : 2049391
Was this helpful?
What can we do to improve the information ?