Technical FAQs

Ask a Question

Can the handle of the 8903 combination style Nema 12/3R device be padlocked in the off postion?

Yes, both handles are padlockable. One handle operates the disconnecting means and can only be padlocked in the off position. The other handle opens and closes the door.


CTA-ID : 2048713
Was this helpful?
What can we do to improve the information ?