Technical FAQs

Ask a Question

Do GJL and NSE circuit breakers have CSA listings?

Issue:
Do GJL and NSE circuit breakers have CSA listings?

Product Line:
Motor Circuit Protector

Environment:


Cause:


Resolution:
As of March, 2009, GJL, GDL, and NSE (NENL) Circuit Breakers no longer carry CSA certification. These breakers will continue to have UL and IEC certification. Affected catalog numbers:
GJL36015 -> GJL 36100, GDL36015 -> GDL36100
NENL34015 -> NENL34100
Motor Circuit Protectors continue to have CSA certification.
GJL36003MO1 through GJL36075M06


CTA-ID : 2049297
Was this helpful?
What can we do to improve the information ?