Technical FAQs

Ask a Question

What is the part number of the retaining kit required for back-feeding a QO breaker in a QO130L200GRB load center?

Issue:
Selection

Product Line:
QO Load Center Accessory

Environment:
Retaining kit selection

Cause:
Select correct accessory

Resolution:
If the back-fed breaker is 125A, or less, use PK4MB2HA. If the back-fed breaker is 150A - 200A, use PK5RK.


CTA-ID : 2050466
Was this helpful?
What can we do to improve the information ?