Technical FAQs

Ask a Question

If there is no voltage available on an undervoltage trip unit on a LX breaker, will the breaker contacts still close momentarily if someone tries to close the breaker( turn it on)?

Issue:
If there is no voltage available on an undervoltage trip unit on a LX breaker, will the breaker contacts still close momentarily if someone tries to close the breaker (turn it on)?

Product Line:
LX, LE, LXI

Environment:

Cause:

Resolution:

The breaker does not have a ``kiss free`` design. Therefore we cannot gurantee the breaker contacts will not touch or close momentarily.


CTA-ID : 2050512
Was this helpful?
What can we do to improve the information ?