Technical FAQs

Ask a Question

Are the 8903 contactors rated for capacitor switching ?

No . Use an 8502S Type S contactor instead. There are also some specific D line contactors marketed internationally for use with capacitors. These are not UL listed.

CTA-ID : 2050706
Was this helpful?
What can we do to improve the information ?