Technical FAQs

Ask a Question

For 8630 reduced voltage, what is the difference between Open transition and Closed transition?

Closed transition consists of an extra contactor and resistor bank that keep the motor windings energized for a few cycles until the transition from wye to delta is complete. An Open transition starter disconnects the motor from the line for a brief period during the transition from Wye to Delta.

CTA-ID : 2050687
Was this helpful?
What can we do to improve the information ?