Technical FAQs

Ask a Question

What are the part numbers for field installable shunt trip accessory for MG, MJ, PG, PJ, PL, RG, RJ, RL Powerpact breakers?

Product Line:
PowerPact M, P, R type circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
Below is list of the shunt trip accessories:

S33658 for 12Vdc
S33659 for 24/30Vac/dc
S33660 for 48/60Vac/dc
S33661 for 100/130Vac/dc
S33662 for 200/250Vac/dc
S33663 for 277Vac
S33664 for 380/480Vac

CTA-ID : 2050564
Was this helpful?
What can we do to improve the information ?