Technical FAQs

Ask a Question

What Class of fuse does the D326NR safety switch accept?

Issue:
Switch features 

Product Line:
General Duty Safety Switches

Environment:
Class of fuse

Cause:
Fuse requirement

Resolution:
This switch accepts as standard a Class H or K fuses when used on a circuit capable of delivering not more than 10,000 RMS symmetrical amps at 240Vac Maximum.
The switch will accept the Class R fuses (field install the Class R Fuse Kit DRK600), when used on a circuit capable of delivering not more than 100,000 RMS symmetrical amperes at 240Vac Maximum.
The switch will accept the Class J fuses, to convert the switch for use with Class J fuses, order kit catalog number GDJK600 separately. Can be used on a circuit capable of delivering not more than 100,000 RMS symmetrical amperes at 240Vac Maximum.



CTA-ID : 2050106
Was this helpful?
What can we do to improve the information ?