Technical FAQs

Ask a Question

Since the FP221R has been obsoleted, what can be used instead for an air conditioning disconnect?

Consider using a QO2L40RB load center and a QO230 circuit breaker, or a QO2TR circuit breaker enclosure and a QO230 circuit breaker. The QO230 circuit breaker is HACR rated.


CTA-ID : 2050602
Was this helpful?
What can we do to improve the information ?